AXIS#.SWLS.LIMIT#
Description
Sets the position value for a software limit switch, LIMIT0 or LIMIT1.
Examples
Usage
If only one limit switch is enabled, AXIS#.SWLS.EN = 1 or 2, then AXIS#.SWLS.LIMIT0 is the lower limit and AXIS#.SWLS.LIMIT1 is the upper limit.
If both limit switches are enabled, AXIS#.SWLS.EN = 3, then whichever switch is set to a larger value is the upper limit switch and the other switch is the lower limit switch.
Code
Axis 1 lower limit switch set to 1000 and upper limit switch set to 5000. Axis 1 home position is set and then both software limit switches are enabled.
-->AXIS1.SWLS.LIMIT0 1000 -->AXIS1.SWLS.LIMIT1 5000 -->AXIS1.HOME.SET -->AXIS1.SWLS.EN 3
Context
For more information on limit switches, refer to Limits.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
| Type | Read/Write |
| Units | Position Units |
| Range | -9,007,199,254,740,992.000 to 9,007,199,254,740,992.000 |
| Default Value | AXIS#.SWLS.LIMIT0 = 0 |
| AXIS#.SWLS.LIMIT1 = 5760 | |
| Data Type | Float |
| See Also | AXIS#.SWLS.STATE, AXIS#.SWLS.EN |
| Stored in Non Volatile Memory | Yes |
Variants Supported
All variants are supported
Fieldbus Information
| FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design | Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
|---|---|---|---|---|---|---|---|---|
| EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen | AXIS1.SWLS.LIMIT0 | 0x500F | 0x3 | DINT | - | Position | RW | False |
| AXIS1.SWLS.LIMIT1 | 0x500F | 0x4 | DINT | - | Position | RW | False | |
| AXIS2.SWLS.LIMIT0 | 0x510F | 0x3 | DINT | - | Position | RW | False |
|
Copyright © 2018 Kollmorgen |
|